Version 0.98.01.01 Released

Update to add full support for SysLink based platforms. Some code refactoring done to make the system more modular (so we can change DSP OS between DSP/BIOS5 and SysBios6, change the IPC mechanism between DSPLink and SysLink, etc.)

Direct Download Link: https://gforge.ti.com/gf/download/frsrelease/642/4970/C6Run_0_98_01_01.tar.gz

Version 0.97.03.03 Released

Bug fixes and some new stuff. In particular, fixes to the front end c6runlib tool so that output names of generated files align with the generated object files. Added regression test cases to verify the front-end tools. Fix the c6x_intrinsic test case to actually run. Changes in memory map for TI816x platform. This is likely to be the last 0.97 release, pending any further bugs.

Direct Download Link: ... (see more)

Version 0.97.02.02 Released

Bug fixes and some new stuff. This latest version now provides support for TI's new IPC layer, called SysLink. In conjunction with this change, SysBios6 replaces DSP/Bios 5 for the platforms that use SysLink. The new SysLink support is primarily intended to support the C6A816x/C6A814x product families, though example platform definitions for DM3730 and OMAP-L138 are included.

Direct Download Link: ... (see more)

Version 0.95.02.02 Released

Important bug fixes for passing buffer arguments to the DSP (passing a pointer in the middle of an allocated buffer should now work). Fix to c6runlib-cc wrapper to properly handle multiple C files at once.

Direct Download Link: https://gforge.ti.com/gf/download/frsrelease/481/4268/C6Run_0_95_02_02.tar.gz

Version 0.95.00.00 Released

Begins some structural changes in preparation to get an SDK-type recipe into Angstrom. Also making changes to adapt to BIOS6 in place of BIOS5, and replace the ARM-DSP communication layer.

Direct Download Link: https://gforge.ti.com/gf/download/frsrelease/445/4143/C6Run_0_95_00_00.tar.gz